Delete a server

If an application or area no longer needs to reference a server, delete the server. To avoid unexpected results, delete a server when the application is not running.
Removing a data server reference deletes server configuration information within the application or area and sub-areas. This includes server name, server ProgID, server location, and references to any related project information.
During run-time operation, rename data servers before deleting and recreating them. There is no need to rename data servers before deleting and recreating them during development.
Prerequisites
Deleting a server requires these permissions for the application or area:
  • Common > Delete
  • Common > List Children
  • Common > Read
To delete a server
  • In
    FactoryTalk Administration Console
    Explorer
    , expand the application tree until the server is visible, right-click the server icon, and then select
    Delete
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal