New Application
How do I open New Application?
- InFactoryTalk Administration ConsoleExplorer, right-clickNetworkorLocal, and then selectNew Application.
An application organizes project information and makes it available to all software products and computers participating in a
FactoryTalk
system.Enter this information to identify the new application.
Setting | Description |
---|---|
Name (required) | In the Name box, type a descriptive name to identify the application. Application names can contain alphanumeric characters, underscores, and spaces. However, names cannot start with an underscore ('_') or a space. |
Description (optional) | In the Description box, enter text to describe the application to its users and provide support information. For example, explain its function, the equipment it operates, the last version installed and support contact information. This information does not appear anywhere else in the FactoryTalk system. |
Provide Feedback