Add an application
To organize project information and make it available to all products in a
FactoryTalk
system, add an application. Add elements such as servers (data servers, HMI servers, and alarm and event servers) and areas to the application. A FactoryTalk
network directory can manage any number of separate network applications. A FactoryTalk
local directory can manage any number of separate local applications.Prerequisites
Adding applications requires these permissions:
- Common > Create Children
- Common > List Children
- Common > Read
To add an application
- InFactoryTalk Administration ConsoleExplorer, right-clickNetworkorLocal, and then selectNew Application.
- InNew Application, type a name and optional description, and then selectOK.Application names can contain alphanumeric characters, underscores, and spaces; however, names cannot start with an underscore ('_') or a space.TIP:
- To add data servers to your application, inFactoryTalk Administration ConsoleExplorer, right-click the application, and then selectAdd New Server.
- To add optional areas to organize a network application, right-click the application, and then selectNew Area.
Provide Feedback