View or edit an application
To help identify the purpose of an application, or to record information about the application, such as contact names or a version history, enter a description of the application.
Use
Application Properties
to view and change its description. The name of the application is read-only.To view or edit an application
- InFactoryTalk Administration ConsoleExplorer, right-click the application, and then selectProperties.
- (optional) InDescription, type a description, and then selectOK.
Provide Feedback