New Logical Name
How do I open New Logical Name?
In the
Explorer
window, expand the FactoryTalk
network or local directory tree until the application or area where you would like to assign the logical name is visible, right-click the area or application, point to Logical Name
, and click New
. Alternately, open
New Logical Name
from the Resources Editor
or the Logical Names
tree in the Explorer
(if available).Use
New Logical Name
to create an alias for the path to a device. A logical name associates security permissions directly with the name, rather than with the path. This allows you to associate a network or device with a single set of security permissions. Devices with identical logical names share security permissions across different control networks and across different computers.
IMPORTANT:
When using
RSLogix 5000®
controllers, you must use logical names to add a mapping between FactoryTalk Administration Console
and the devices.After creating a new logical name, type a descriptive name to identify it.
- IfNew Logical Nameis opened from an application or area inFactoryTalk Administration ConsoleExplorer, the new logical name is assigned to the application or area.
- IfNew Logical Nameis opened fromSelect Resources, useLogical Name Propertiesto assign the new logical name to an application or area.
How to add or delete a logical name
Provide Feedback