Delete a logical name from an area or application
Delete a logical name from an area or an application to break the link between the logical name and the permissions associated with the area or application.
For how to add the logical name, see Add a logical name to an area or application.
Prerequisites
Deleting a logical name requires these permissions for the application or area:
- Common > Delete
- Common > List Children
- Common > Read
To delete a logical name from an area or application
- InFactoryTalk Administration ConsoleExplorer, expand the local or network directory tree until the application or area that contains the logical name is visible.
- Right-clickthe application or area icon, and then selectResource Editor.
- In theResources Editor, the application is selected in theAreaslist.
- In theAssociated Resourceslist, select the logical name to delete, and then selectCut.
- SelectClose.
Provide Feedback