Add a logical name to an area or application
Devices with identical logical names share security permissions across different control networks and across different computers, even if those devices are configured with different driver names or network paths. Add logical names before configuring security for
RSLogix 5000
controllers. For all other types of control hardware, choose whether to associate security settings with logical names or with network relative paths. Add a logical name to an area or application when the permissions associated with the logical name are inherited from that area or application. For how to delete the logical name, see Delete a logical name from an area or application.
Prerequisites
Adding a logical name requires these permissions for the area or application:
- Common > Create Children
- Common > List Children
- Common > Read
To add a logical name to an area or application
- InFactoryTalk Administration ConsoleExplorer, right-click the application or area, point toLogical Name, and then selectNew.
- InNew Logical Name, type a name and selectOK.
Provide Feedback