Resources Editor
How do I open Resources Editor?
- StartFactoryTalk Administration ConsoleorFactoryTalk View Studioand then log on to theFactoryTalkNetwork Directory orFactoryTalkLocal Directory where the resource groupings to modify are located.
- In theExplorerwindow, right-click any application or area and selectResource Editoron the context menu.
Use
Resources Editor
to edit a resource grouping in an area or application. Select Manage Resources
to add or remove resources, or to map resources to logical names.Setting | Description |
---|---|
Areas | Displays the applications and areas in the FactoryTalk network directory, or the applications in the FactoryTalk local directory. Select an area or application to view the list of resources associated with it. |
Associated resources | Shows the hardware devices located in the application or area. Devices that are represented by logical names are displayed using their logical names. Devices that are represented by network relative paths are shown by their network relative paths.
|
Manage Resources | Select Manage Resources to add or remove resources in the selected application or area, or to map resources to logical names. |
Provide Feedback