Manage resource groupings

A resource grouping is a collection of hardware resources from the
Networks and Devices
tree that is associated with an application or area. Grouping hardware resources under an application or area allows defining of security permissions for a set of control hardware in one step, rather than having to set permissions for each device separately. Hardware in a resource grouping can be defined by its network relative path or by its logical name.
To manage the security of control hardware through an application or area, use the
Resources Editor
to:
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal