Move a resource between areas

Use the
Resources Editor
to move a hardware resource from one application or area to another. The device or control network that is moved inherits the security permissions of its new area or application.
Prerequisites
Moving hardware resources between areas requires these permissions for the application or area:
  • Common > Read
  • Common > List Children
  • Common > Configure Security
To move a resource between areas
  1. In
    FactoryTalk Administration Console
    Explorer
    , right-click any application or area and then select
    Resource Editor
    .
  2. In the
    Areas
    list, select the area containing the resource to copy.
  3. In the
    Associated resources
    list, right-click the resource, and then select
    Cut
    .
  4. In the
    Areas
    list, select the area to copy the resource to, right-click the
    Associated resources
    list again, and then select
    Paste
    .
  5. When finished, select
    Close
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal