Resource groupings

A resource grouping is a collection of hardware resources from the
Networks and Devices
tree that is associated with an application or area. A resource grouping is not a separate account type.
Grouping resources under an application or area allows granting or denying security permissions for a set of control hardware in one step, rather than setting permissions for each device separately.
Create a resource grouping in any application or area in the
FactoryTalk Directory
by selecting resources to associate with the area in the
Resources Editor
. A resource grouping automatically inherits the security settings of the application or area where the resource group is located.
These security permissions might be explicit permissions defined specifically for the area, or they might be inherited from the application in which the area is located, or from the
FactoryTalk Directory
in which the application is located. If needed, set explicit permissions for a device that override the security permissions set for its resource group by browsing for the network or device in the
Networks and Devices
tree.
To prevent conflicting permissions, these configurations are not permitted:
  • Nesting resource groupings within other resource groupings.
  • Including the same network or device in multiple resource groupings within the same
    FactoryTalk Directory
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal