Select Resources

Use
Select Resources
to associate resources with an application or area. Referenced the hardware devices by logical name or by network relative path. Use these settings to specify how resources are added to the grouping.
Setting
Description
Select resources to be associated with an area
  • To view the logical names for only those devices that are not already associated with an application or area, select
    Show only logical names not associated with areas
    . Ignore this setting if not using logical names with networks and devices.
  • To view all logical names, even those already associated with an application or area, select
    Show all logical names
    . Ignore this setting if not using logical names with networks and devices.
  • To add a logical name to the list of resources in the grouping, select the logical name and select
    >
    . The same network or device (represented by a logical name) cannot be added to multiple resource groupings.
  • To add a device using its network relative path, expand the
    Networks and Devices
    tree until the device is visible. Select the device and select
    >
    . The same network or device cannot be added to multiple resource groupings.
Add New Logical Name
Select to create a new logical name for a device.
Delete Logical Name
Delete logical names that are no longer in use in the system, but remain visible in this dialog box. This occurs if the device associated with a logical name was deleted.
Delete Logical Name
is disabled if the selected logical name is in use.
Selected resources
Shows the resources that are associated with the application or area. To remove a resource from the list, select the resource and select
<
.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal