Add a server to an area or application
A
FactoryTalk Directory
holds any number of applications and servers, such as data servers, device servers, alarm and event servers, and HMI servers. Add a server to an application or an area to create a link between the server and the FactoryTalk Directory
. Add these servers to either an application or an area:
Prerequisites
Adding a server requires these permissions for the application or area:
- Common > Create Children
- Common > List Children
- Common > Read
To add a server to an area or application
- InFactoryTalk Administration ConsoleExplorer, right-click the application or area, point toAdd New Server, and then select either:
- Rockwell AutomationDevice Server (FactoryTalk Linx)
- OPCDA Data Server
- Tag Alarm and Event Server
- (skip to step 9)OPCUA Server (FactoryTalk Linx OPC UA Connector)
- InGeneral Server Properties, name the server and identify the computer that hosts the server.
- (optional) Add a description of the server.
- Edit other properties on theGeneraltab as needed.
- . InFactoryTalk LinxServer PropertiesServer Typeselect either:. The mainFactoryTalk LinxBase ServerFactoryTalk LinxServer that supports all the functions ofFactoryTalk Linx.. A supplementalFactoryTalk LinxExtended ServerFactoryTalk LinxServer that extends that number of tags, data client, and/or controllers that an application or area can support.
- OPC Data Server Properties. InOPC Server name (ProgID)browse to choose the OPC data server.If adding a data server to a network application, chooseRSLinx Remote OPC Server, if adding a data server to a local application, chooseRSLinx OPC Server.
- Tag Alarm and Event Server Properties. InStartup type, choose how the Tag Alarm and Event Server starts up.SelectLoad when operating system initializesto start the Tag Alarm and Event Server automatically when the computer starts up. This option should be used in all running systems.SelectWhen first client connects (Redundancy will be disabled)to start the Tag Alarm and Event Server when the first client connects to the server. Selecting this option disables redundancy so it should only be used in certain circumstances to prevent service conflicts, such as when:
- Testing several alarm servers on the same computer.
- Restoring an existing application which contains Tag Alarm and Event Servers.
- Configure the properties on theRedundancytab to set up options for a secondary server to use if the primary server fails.
- SelectProvide redundancy using a secondary serverto enable server redundancy and to activate the redundancy options.
- Specify the name of the computer on which the secondary server will run. InComputer running the secondary serverbrowse or type the name of the secondary server.Choose a switch-over option:
- SelectContinue using the secondary server even when the primary server becomes available againto continue using the secondary server after the switch over occurs. Use this option to bring the primary server back online to diagnose and correct the problems on the computer that failed before returning it to use as the primary server.
- SelectSwitch over to the primary data server when it becomes available againto immediate return to using the primary server when it becomes available. Use this option to switch between servers during scheduled hardware maintenance or approved software updates that do not require server functional verification before returning the server to operation.
- If adding aconfigure the properties on theRockwell AutomationDevice Server (FactoryTalk Linx)Alarms and Eventstab to enable or disable alarm and event support, to edit the settings for server-assigned priorities, and to enable alarm and event history logging.
- If adding anon theOPCDA Data ServerAdvancedtab select whether to create a cache of the data server's tag names and to include extended tag information in the cache.
- If adding aTag Alarm and Event Server,configure the properties on thePriorities and Historytab to define alarm severity-to-priority settings for an individual server.
- If adding an, theOPCUA Server (FactoryTalk Linx OPC UA Connector)FactoryTalk Linx OPC UA Connectorproperties display:
- InConnector Settingsenter values for:
- Name:Enter a unique name for this Connector. The Connector name displays in the FactoryTalk application tree and is included in the full tag path for all tags provided by the Connector.
- Computer hosting the FactoryTalk Linx OPC UA Connector:Type the hostname, IP address, or fully qualified domain name, or browse to select the remote host computer. The remote host computer must have FactoryTalk Services Platform installed. Both the remote host computer and the client computer must be configured to use the same FactoryTalk Services Platform Network Directory host.
- SelectOPC UA Serversand enter values for:
- Name:Enter a unique name for the OPC UA Server. The server name displays in the FactoryTalk application tree and is included in the full tag path for all tags provided by the server.
- (optional)Description:Enter a description for the OPC UA Server.
- Endpoint URL:Enter the full network path or IP address or select browse to select the OPC UA Server. The path must be in the format opc.tcp://hostname_or_ip:port/Path/To/Server where hostname_or_ip, port, and /Path/To/Server are replaced with the OPC UA Server settings.The firewall on the OPC UA Server must allow incoming connections to the selected port for the connection to succeed.
- (optional) SelectAddand then repeat step (b) for each OPC UA Server used to provide tags to FactoryTalk applications through this FactoryTalk Linx OPC UA Connector.
- Once finished, selectOK.
Provide Feedback