Add a FactoryTalk Linx server
Add a
FactoryTalk Linx
server to add references to device servers within applications to an application or an area.To access both tag values and alarm and event values from a
ControlLogix®
processor, use direct references to the processor through a Rockwell Automation
Device Server (FactoryTalk Linx
).Prerequisites
Adding a
FactoryTalk Linx
server requires these permissions for the application or area:- Common > Create Children
- Common > Write
- Common > Read
To add a
FactoryTalk Linx
server- InFactoryTalk Administration ConsoleExplorer, right-click the application or the area name, point toAdd New Server, and then select.Rockwell AutomationDevice Server (FactoryTalk Linx)
- InGeneral Properties, useBrowseto locate the computer where the server resides. To save your changes, selectApply.
- (optional) On theRedundancytab, set up options for a secondary server, should the primary data server fail. To save your changes, selectApply.
- (optional) On theAlarms and Eventstab, set up options for assigning alarm priorities and logging historical alarm and event data. To save your changes, selectApply.
- When you finish setting up server options, selectOK.
- Next, create shortcuts to establish communications between the server and hardware devices. InFactoryTalk Administration ConsoleExplorer, expand theFactoryTalk Linxdevice server, right-clickCommunication Setupand selectOpen. The content pane displays these areas:
- Device Shortcuts
- Primary tab
- Offline Tag File
- On thePrimarytab add the devices from which the application will receive data.
- InDevice Shortcuts, useAddto add device shortcuts that represent routes to the devices. When finished, selectOK.TIP:When setting up a device shortcut inFactoryTalk Linxspecify an offline tag file to use an offline copy of the tags in the controller when the controller is unavailable.
Provide Feedback