General FactoryTalk Linx Server Properties

How do I open General
FactoryTalk Linx
Server Properties?
  1. In
    Explorer
    , expand applications or areas until the
    FactoryTalk Linx
    server is visible.
  2. Right-click the
    FactoryTalk Linx
    server, then select
    Properties
    .
Use
FactoryTalk Linx
Server General Properties
to configure the name, description, and location of a
FactoryTalk Linx
server.
Setting
Description
Name
Shows the
FactoryTalk Linx
server name. This name cannot be changed after the server is created and cannot include dashes or hyphens (–).
Description
Enter a description for the
FactoryTalk Linx
server. For example, use this box to describe a component's location, to identify a contact person or number in the event of failure, or to keep track of changes or version information.
Computer hosting the
FactoryTalk Linx
server
For local applications, displays the name
localhost
as the computer hosting the
FactoryTalk Linx
server. This indicates that the
FactoryTalk Linx
server will execute on the local computer. When configuring a local application, this property cannot be changed.
For network applications, displays the computer name of the local computer. If the
FactoryTalk Linx
server is not being hosted on the local computer, enter a different computer name, or select
Browse
to specify another computer.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal