General Application Properties

How do I open General Application Properties?
  • In the
    Explorer
    window, right-click an application icon and select
    Properties
    .
In
Description
, enter text to describe the application. For example, explain its function, the equipment it operates, support information, or version history. This information does not appear anywhere else in the FactoryTalk system. It can be updated as needed to reflect the current state of the application.
The name of an application cannot be changed.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal