Parameters tab

Parameters are listed alphabetically by default. Group parameters make organization and access more intuitive.
  • Group names display in blue. Group names display in this format:
    library object Name [Group Name]
    .
  • Collapse and expand the group using the arrow buttons on the right, or by double-clicking the group name. Parameters display alphabetically within their groups, although the display order can be changed.
  • When a new library object is added, an initial group is created in the
    Parameters
    tab. The group name matches the library object name. Additional groups can be added as parameters are added to the library object.
  • Subobjects appear in the
    Parameters
    tab as a type of group. Subobject names display in blue. Subobject names are displayed in this format:
    library object Name.SubObject Type
    .
This table describes the commands available on the
Parameters
tab toolbar.
Command
Description
Add New icon
The
Add New
button opens the
Add New Parameter
window.
Move Up icon Move Down icon
The
Move Up/Move Down
buttons change the position of a selected Parameter item in the tab listing. Parameters are listed in alphabetical order by default. Parameters may be moved up or down within their group but cannot be moved between groups using these buttons.
Find partial
This dropdown menu can initiate a search for parameters that match a text string entered in the adjacent field. There are two different types of finds that can be performed, use the dropdown menu to select the one to use:
  • FindPartial
    : Searches for the text string in any part of an entry.
  • FindPrefix
    : Searches for the text string at the beginning of an entry.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal