Add a parameter

A parameter is an argument exposed for external access and controls how the library object is instantiated. Parameters allow a single instance of base controller code to have many variations and are used in a variety of different applications.
To add a parameter
  1. In the decorator panel, either:
    • Click Add New icon on the
      Parameters
      tab toolbar.
    • In the
      Parameters
      tab, right-click a group name and then click
      Add New Parameter
      .
      The Add New / Edit Parameter window opens.
      TIP:
      The entry fields in the window are functionally grouped. Some fields appear conditionally based on selections made in other fields.
  2. Enter the values for the new parameter.
  3. Click
    OK
    to add the new parameter.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal