Add a subobject

A subobject is a grouped set of parameters that can be instantiated multiple times. Subobjects can be auto-generated during instantiation or added manually by the user when the library object is brought into an
Application Code Manager
project.
To add a subobject
  1. In the decorator panel, right-click any group name, then select
    Add New SubObject
    .
    The New SubObject window opens.
  2. Enter the values for the new subobject.
  3. Click
    OK
    to add the new subobject.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal