View a parameter reference
Use the
References
window to view a list of all references to a parameter. A
reference makes the value of a tag or element within a library object accessible to
parameters in other library objects. From the References
window, navigate to the
referencing entities to view tag details.To view a parameter reference
- In theLibrary Objectspane, click the library object that contains the parameter of interest.
- In the decorator pane, on theParameterstab, right-click the parameter and then clickShow References. The References window opens.
- ClickNavigatefor the reference listing. The decorator pane updates to display the tag details for that element.
- ClickOKto close theReferenceswindow.TIP:TheReferenceswindow must be closed before the items in the decorator panel can be accessed.
Provide Feedback