References window
How do I open the
References window?
To open the
References
window for a parameter, right-click the parameter to open the
contextual menu, then select Show References
.Once a parameter, substitution, or function is added to a library object, it may be referenced multiple times within the library object. Parameters, substitutions, or functions added to a project or controller library object may be referenced from within multiple library objects.
Examples of ways references can be used:
- As a part of a field value
- As part of an expression
- As part of a substitution
- As part of a function
The
References
window lists all references to the selected item and navigates to the referencing entities.The fields in the
References
window.Name | Description |
|---|---|
Library | The library object for the element that references the item. |
Used by | The element that references the item. The value is displayed in this format: Element Type:SubObject Name . |
Details | The specific reference point within the element. For example, a field in the Edit Parameter window, a conditional inclusion, or the Value Expression for a controller or local tag. |
Navigate | Click to open the decorator panel for the element where the reference is located. |
Provide Feedback