Edit a parameter
Parameters allow a single instance of base controller code to have many variations and are used in a variety of different applications.
To edit a parameter
- In the decorator pane, click theParameterstab, either:
- Double-click the parameter.
- Right-click the parameter, then selectEdit.
- TheEdit Parameterwindow opens.
- Enter the values for the edited parameter.
- ClickOKto update the parameter.
Provide Feedback