Copy a parameter
A parameter must be unique within a library object. A parameter can be copied to other library objects and to library objects of different scope.
To copy a parameter
- In the decorator pane, right-click the parameter, then selectCopy.Select multiple parameters by pressing theShiftorCtrlkey while clicking.
- In theLibrary Objectspane, click the library object to which to add the parameter.
- In the decorator pane, right-click the name of the group in theParameterstab and then clickPaste Parameter(s).The parameter is added to the library object.TIP:The parameter retains its original group name, so a new group might also be added along with the parameter.
Provide Feedback