Move a parameter within a group
Parameters can be collected together into a group. The order of the parameters in the group determines the order in which each parameter is instantiated.
To move a parameter within a group
- In the decorator panel, on theParameterstab, click the parameter.
- After selecting the parameter, either:
- On theParameterstoolbar, clickMove UporMove Down.
- Right-click the parameter, then selectMove UporMove Down.TIP:A parameter cannot be moved outside of its group. To change the group membership, reassign the parameter.
Provide Feedback