Delete a parameter

Delete parameters that are not used. If a parameter is used in a reference, it cannot be deleted. Use the
Show References
command to view parameter references before attempting to delete a parameter.
To delete a parameter
  1. Right-click the parameter, then select
    Delete
    .
    The
    Delete Objects
    dialog opens.
  2. To finish the deletion, click
    Yes
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal