Reassign a parameter to a group
Parameter groups are added, modified, and deleted through the
Group
setting in the Add New Parameter
and Edit Parameter
windows. Changing the Group setting of a parameter reassigns it to another group or creates a group if the group specified does not exist. To reassign each parameter in a group, edit each parameter individually.To reassign a parameter
- In the decorator pane, click theParameterstab, then either:
- Double-click the parameter.
- Right-click the parameter, then selectEdit.
- TheEdit Parameterwindow opens.
- Under theUserInterfacesection, inGroup, type a new name or a name of an existing group.TIP:When reassigning parameters to existing groups, make sure to type the group name exactly as it appears in theParameterstab.
- ClickOKto reassign the parameter.
Provide Feedback