Add a group

All groups other than the default group must contain at least one parameter. Parameter groups are added, modified, and deleted through the
Group
setting in the
Add new Parameter
and
Edit Parameter
windows.
When the
Group
setting is blank, the default Group name is based on the name of the library object. To use a different default group name, add text to the
Group
setting of the first parameter added to the library object, the text is appended to the library object name. Subsequent parameters added will use that group name by default. If the
Group
setting is edited to be blank in any parameter, the original default group name based on the library object name is re-established.
To add a group
  1. In the decorator panel, either:
    • Click Add New icon on the
      Parameters
      tab toolbar. The
      Add New Parameter
      window opens.
    • Double-click an existing parameter that does not belong to a group. The
      Edit Parameter
      window opens.
  2. Under the
    UserInterface
    section, in
    Group
    , type a name.
  3. Click
    OK
    . A new group is created, and the parameter is included in the new group.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal