Add an external reference

An external reference makes the value of a local tag, controller tag, or tag member within a library object accessible to parameters in other library objects.
IMPORTANT:
While all of the fields in the References Builder are open to manual editing, it is recommended to follow this procedure and allow the
Library Designer
to enter values automatically.
To add an external reference
  1. Locate the tag within the library object.
    TIP:
    Controller tags and local tags are open for use as external references.
  2. Double-click the tag name. The name highlights to indicate it has been selected.
  3. Right-click the selected tag name, then select
    Add External Reference
    .
    The
    References Builder
    window opens.
  4. Enter the values for the new external reference or accept the default values generated by
    Library Object Manager
    .
  5. Click
    OK
    to add the external reference.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal