EtherNet/IP Register Map

All EtherNet/IP Parameters in the register map can be accessed via explicit controller messaging via a generic CIP message block in Rockwell Studio 5000. The class ID for all Parameters will be
0xA2
in hex with the Instance ID corresponding to the Register Map Instance ID value. Please note that the Register Map tables may not match the EDS file groups parameters, and some parameters may only be kept in reservation for future use.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal