Offset Register Map

The Offset Register map contains parameters used by the PQconnect board for factory calibration of the PCB and the Users Unit for offsetting any current, voltage, and temperature readings.
Note that some parameters shown below may not exist in the parameter database/ or shown in PQVision. These parameters have been reserved for future use.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Parameters should not be changed manually by the user, doing so will alter the filter’s performance and accuracy.
Table
13
: Offset Feedback and Setpoint Parameters Register Map
Parameter Name (EtherNet/IP Name)
Instance ID
Description
Type
Default & Ranges
Notes
V_THD_OFFSET (VTHDOffset)
117
Voltage THD offset adjustment factor
R/W
Default:0
Range: -32768 to 32767
Value set by Factory
I_THD_OFFSET (ITHDOffset)
118
Current THD offset adjustment factor
R/W
Default:0
Range: -32768 to 32767
V_LOAD_B_OFFSET (VLoadBOffset)
120
Load voltage offset phase B
R/W
Default:0
Range:0 to 0
EtherNet Only: Reserved Does not exist in Database
V_LINE_A_OFFSET (VLineAOffset)
121
Line voltage offset phase A
R/W
Default:2048
Range:0 to 4096
Value set by Factory
V_LINE_B_OFFSET (VLineBOffset)
122
Line voltage offset phase B
R/W
Default:2048
Range:0 to 4096
V_LINE_C_OFFSET (VLineCOffset)
123
Line voltage offset phase C
R/W
Default:2048
Range:0 to 4096
V_LOAD_A_OFFSET (VLoadAOffset)
124
Load voltage offset phase A
R/W
Default:2048
Range:0 to 4096
V_LOAD_C_OFFSET (VLoadCOffset)
125
Load voltage offset phase C
R/W
Default:2048
Range:0 to 4096
V_TUNE_A_OFFSET (VTuneAOffset)
126
Tune voltage offset phase A
R/W
Default:2048
Range:0 to 4096
V_TUNE_C_OFFSET (VTuneCOffset)
127
Tune voltage offset phase C
R/W
Default:2048
Range:0 to 4096
V_DIFF_LINE_A_OFFSET (VRctrLineAOffset)
128
Reactor Diff Voltage Offset Phase A
R/W
Default:2048
Range:0 to 4096
V_DIFF_LINE_B_OFFSET (VRctrLineBOffset)
129
Reactor Diff Voltage Offset Phase B
R/W
Default:2048
Range:0 to 4096
V_DIFF_LINE_C_OFFSET (VRctrLineCOffset)
130
Reactor Diff Voltage Offset Phase C
R/W
Default:2048
Range:0 to 4096
V_DIFF_TUNE_A_OFFSET (VRctrTuneAOffset)
131
Reactor Diff Voltage Offset Phase A
R/W
Default:2048
Range:0 to 4096
V_DIFF_TUNE_B_OFFSET (VRctrTuneBOffset)
132
Reactor Diff Voltage Offset Phase B
R/W
Default:2048
Range:0 to 4096
V_DIFF_TUNE_C_OFFSET (VRctrTuneCOffset)
133
Reactor Diff Voltage Offset Phase C
R/W
Default:2048
Range:0 to 4096
I_LINE_A_OFFSET (ILineAOffset)
134
Line Current Offset Phase A for CT Input
R/W
Default:2048
Range:0 to 8192
Value set by Factory
I_LINE_C_OFFSET (ILineCOffset)
135
Line Current Offset Phase A for CT Input
R/W
Default:2048
Range:0 to 8192
I_LOAD_A_OFFSET (ILoadAOffset)
136
Load Current Offset Phase A for CT input
R/W
Default:2048
Range:0 to 8192
I_LOAD_C_OFFSET (ILoadCOffset)
137
Load Current Offset Phase A for CT input
R/W
Default:2048
Range:0 to 8192
T_AMBIENT_OFFSET (TCtrlOffset)
138
Offset for controls temperature
R/W
Default:683
Range: -8192 to 8192
V_DIFF_LINE_A_SCALAR (VReactorLineScalarA)
139
Line reactor voltage scalar phase A
R/W
Default:16384
Range: -32768 to 32767
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal