Control Register Map

This register map contains parameters which are used to control the Harmonic Guard filter. Note that some parameters shown below may not exist in the parameter database/ or shown in PQVision. These parameters have been reserved for future use and are enabled in EtherNet/IP EDS File.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Table 3: Control Feedback and Setpoint Parameters Register Map
Parameter Name
(EtherNet Name)
Instance ID
Description
Type
Default & Ranges
Notes
T_AMBIENT
(TControl)
276
Filter controls temperature
R
Default:0
Range: -75C to 75C
Board will give a status condition of overtempt if it exceeds 75C or under-temp if the temperature descends past -40C.
10 = 1.0 deg C
Range: -75C to 75C
SYS_INIT_COMPLETE
(InitCmpl)
277
Controls start up init and calibration check complete
R
Default:0
EtherNet/IP Only:
Reserved
Does not exist in Database
CAP_DEGREDATION_WARNING
(CapWrn)
278
Filter capacitor degradation warning
R
Default:0
EtherNet/IP Only:
Reserved
Does not exist in Database
SYS_DS_MODE
(DSMode)
291
Data simulation mode active
R
Default:0
Indicates if the Processor is in data simulation mode
0 = Not in Data Sim Mode
1 = Data Sim Mode
CONFIG_MODE_ACTIVE
(ConfigModeActive)
292
Active feedback sensing configuration mode
R
Default:0
Indicates PQconnect board current sensing mode.
0 = Config Sensing Mode Null
1 = Config Sensing Mode is Auto Selecting
2 = Config Sensing Mode is ABC (Uses all 3 phases for sensing, 8 op-amp configuration)
3 = Config Sensing Mode is AC (Uses Phase A and C for sensing, uses 6 op-amp configuration)
SYS_NULL_TMR
(PCBCalTimer)
297
Factory PCB calibration timer value
R
Default:0
System null timer - Indicates whether the unit is calibrating.
In units of 10s of milliseconds (600 = 6 seconds)
SYS_USAGE_MIN
(CtrlCycMin)
301
Controls processor minimum cycle time usage,
(10 = 1.0%)
R
Default:0
SYS_USAGE_MAX
(CtrlCycMax)
302
Processor Max Cycle Usage,
(10 = 1.0%)
R
Default:0
SYS_USAGE_AVG
(CtrlCycAvg)
303
Processor Avg Cycle Usage,
(10 = 1.0%)
R
Default:0
PARAM_USER_CMD_REQ
(ParamCmd)
1
Parameter save/load command
R/W
Default:1
Range:0 to 300
Note
that defaulting the flash will clear all calibration data and require that the calibration procedure be re-run.
0 = Init State
1 = Stop Update
9 = Save Curnt. Values to Flash
21 = Set User Access
25 = Set Tech Access
30 = Set Factory Access
42 = Reboot/Reset PQconnect
100 = Clear History Log
150 = Load Values from Flash
200 = Restore Defaults to Flash
255 = Erase All Calibration Data
300 = Erase Unit Calibration Data
TRACE_GO_DONE
(WaveformTrigCmd)
2
Waveform capture trigger command
R/W
Default:0
Range:0 to 1
Indicates whether waveform data is being captured
0 = Capture Done
1 = Start Capture
SYS_RESET
(ResetCmd)
3
Contactor reset command
R/W
Default:0
Range:0 to 1
Reset contactor
0 = No Command
1 = Reset Contactor Closed
SYS_CONTROL_MODE
(ControlMode)
8
Contactor control mode
R/W
Default:2
Range:0 to 6
Contactor Control Mode
Allows the user to keep the contactor always off/on, auto turn on/off based on desired load percentage or kVAR, external relay input, in debug close mode.
0 = Always Open
1 = Always Closed
2= Auto load
3 = Auto kVAR
4 = External Control Input
5 = No contactor
6 = Diagnostic Always Close
SYS_AUTO_CONTACTOR_CLOSE
(AutoCloseEn)
9
Enable contactor auto to reclose
R/W
Default:0
Range:0 to 1
Contactor auto reclose, this will attempt to reclose the contactor after it has been open through a status condition
0 = Disable
1 = Enable
CNT_CLOSE_LOAD_THRESHOLD
(CntCloseLoadThrsh)
23
Contactor close threshold in load control mode
R/W
Default:30
Range:10 to 100
Contactor close threshold in percent rated current*
% rated current
CNT_CLOSE_LOAD_HYSTERESIS
(CntCloseLoadHys)
24
Contactor close/open hysteresis in load control mode
R/W
Default:5
Range:2 to 50
Contactor will open when it reaches the hysteresis *
% rated current
CNT_CLOSE_DELAY
(CntCloseDelay)
27
Contactor close delay time
R/W
Default:5
Range:1 to 3600
second
CNT_OPEN_DELAY
(CntOpenDelay)
28
Contactor open delay time
R/W
Default:5
Range:1 to 3600
second
CNT_AUTO_RECLOSE_DELAY
(CntAutoReCloseDelay)
31
Contactor auto re-close delay time
R/W
Default:300
Range:120 to 65535
second
CNT_POWER_ON_DELAY
(PowerOnDelay)
32
System power on start delay time
R/W
Default:0
Range:0 to 65535
CNT_AUTO_RECLOSE_ATTEMPTS
(CntAutoReCloseNum)
33
Contactor auto re-close max number attempts allowed
R/W
Default:5
Range:1 to 15
Maximum number of contactors auto re-close attempts allowed
CNT_AUTO_RECLOSE_TIMESPAN
(CntAutoReCloseTime)
34
Contactor auto re-close max attempt time span, (sec)
R/W
Default:600
Range:300 to 65535
Maximum number of contactors auto re-close attempts time span
BOOTLOADER_START
(BootCmd)
39
Bootloader command
R/W
Default:0
Range:0 to 2
Used to navigate to bootloader, which launches the main program
0 = No Action
1 = Start Bootloader
2 = Start Recovery
SYS_MAG_CAL_ENABLE
(UnitCalEn)
78
System magnitude Calibration
R/W
Default:0
Range:0 to 1
System Magnitude Calibration
0 = Disable
1 = Enable
SYS_CNT_MIN_OFF_TIME
(CntMinOffTime)
113
Contactor minimum open time, (sec)
R/W
Default:60
Range:10 to 300
SYS_NULL_EN
(PCBCalEn)
119
Factory PCB calibration enable
R/W
Default:0
Range:0 to 1
PCB Calibration
0 = Disable
1 = Enable
SYS_CPU_THRESHOLD
(CtrlFaultOnset)
159
Controls Processor fault threshold
R/W
Default:12369
Range:0 to 17361
FIELD_BUS_COMMAND
(FBCmd)
180
Field Bus communication module command input
R/W
Default:0
Range:0 to 255
Field Bus Command Input
0 = No Command
3 = Reset
5 = Shutdown
CT_ENABLE
(CTEn)
184
Current transformer CT feedback enable
R/W
Default:0
Range:0 to 1
Only used for filters with dual tuned circuits
0 = Disabled
1 = Enabled
CONFIG_MODE
(SensingFdbkMode)
187
Feedback sensing configuration mode selection
R/W
Default:1
Range:1 to 3
FAULT_PHASE_ROTATION (PhaseRotationDetect)
74
Phase rotation status setpoint
R/W
Default:1
Range:0 to 2
Filter expected input phase orientation
0 = Undef
1 = Forward
2 = Reverse
STATUS_CPU_ERROR_DELAY (CtrlFaultDelay)
157
Controls Processor fault delay time, (Sec)
R/W
Default:0
EtherNet/IP Only:
Reserved
Does not exist in
Database
HISTORY_LOG_REQUEST
(HistReqCmd)
189
Status detection history record request command
R/W
Default:0
Range:0 to 0
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal