Calibration Reference Register Map

The Calibration Reference Register map contains parameters used by the PQconnect board for factory calibration of the PCB and the Users Unit. Note that some parameters shown below may not exist in the parameter database/ or shown in PQVision. These parameters have been reserved for future use.
Note:
All parameters with an asterisk (*) in the description will require the Tech level access codes parameter key A: 0x007D (125) and parameter key B: 0xEA6E (60014). All parameters are enabled for communication to EtherNet/IP unless explicitly stated otherwise in the Notes Column of the Table.
Parameters should not be changed manually by the user, doing so will alter the filter’s performance and accuracy.
Table
12
: Calibration Reference Feedback and Setpoint Parameters Register Map
Parameter Name (EtherNet/IP Name)
Instance ID
Description
Type
Default & Ranges
Notes
SYS_I_LINE_CAL_A (ILineCalRefA)
79
Reference calibration current line phase A,
(10 = 1.0A)
R/W
Default:0
Range:0 to 65535
Input current measured on A phase of the filter
SYS_I_LINE_CAL_B (ILineCalRefB)
80
Reference calibration current line phase B,
(10 = 1.0A)
R/W
Default:0
Range:0 to 65535
Input current measured on B phase of the filter
SYS_I_LINE_CAL_C (ILineCalRefC)
81
Reference calibration current line phase C,
(10 = 1.0A)
R/W
Default:0
Range:0 to 65535
Input current measured on C phase of the filter
SYS_I_TUNE_CAL_A (ITuneCalRefA)
82
Reference calibration current tune phase A,
(10 = 1.0A)
R/W
Default:0
Range:0 to 65535
Tune circuit current measured on A phase of the filter
SYS_I_TUNE_CAL_B (ITuneCalRefB)
83
Reference calibration current tune phase B,
(10 = 1.0A)
R/W
Default:0
Range:0 to 65535
Tune circuit current measured on B phase of the filter
SYS_I_TUNE_CAL_C (ITuneCalRefC)
84
Reference calibration current tune phase C,
(10 = 1.0A)
R/W
Default:0
Range:0 to 65535
Tune circuit current measured on C phase of the filter
SYS_MAG_CAL_TOL (CalTolerance)
85
Current calculation magnitude calibration tolerance,
(10 = 1.0A)
R/W
Default:5
Range:0 to 15000
System mag calibration Tolerance Value used by the PQconnect for setting the threshold for Calibrated reference currents.
Pass/Fail range.
20 = 0.02 amps tolerance
I_LINE_EST_A_INT_DECAY (ILineEstDecayA)
145
Line current estimation decay phase A
R/W
Default:16375
Range:0 to 65535
Value set by Factory
I_LINE_EST_B_INT_DECAY (ILineEstDecayB)
146
Line current estimation decay phase B
R/W
Default:16375
Range:0 to 65535
I_LINE_EST_C_INT_DECAY (ILineEstDecayC)
147
Line current estimation decay phase C
R/W
Default:16375
Range:0 to 65535
I_TUNE_EST_A_INT_DECAY (ITuneEstDecayA)
148
Tune current estimation decay phase A
R/W
Default:16375
Range:0 to 65535
I_TUNE_EST_B_INT_DECAY (ITuneEstDecayB)
149
Tune current estimation decay phase B
R/W
Default:16375
Range:0 to 65535
I_TUNE_EST_C_INT_DECAY (ITuneEstDecayC)
150
Tune current estimation decay phase C
R/W
Default:16375
Range:0 to 65535
I_LINE_EST_A_SIN_NULL (ILineEstCalA)
151
Line current estimation calibration sine phase A
R/W
Default:0
Range: -32768 to 32767
I_LINE_EST_B_SIN_NULL (ILineEstCalB)
152
Line current estimation calibration sine phase B
R/W
Default:0
Range:-32768 to 32767
Value set by Factory
I_LINE_EST_C_SIN_NULL (ILineEstCalC)
153
Line current estimation calibration sine phase C
R/W
Default:0
Range:-32768 to 32767
Value set by Factory
I_TUNE_EST_A_SIN_NULL (ITuneEstCalA)
154
Tune current estimation calibration sine phase A
R/W
Default:0
Range:-32768 to 32767
Value set by Factory
I_TUNE_EST_B_SIN_NULL (ITuneEstCalB)
155
Tune current estimation calibration sine phase B
R/W
Default:0
Range:-32768 to 32767
Value set by Factory
I_TUNE_EST_C_SIN_NULL (ITuneEstCalC)
156
Tune current estimation calibration sine phase C
R/W
Default:0
Range:-32768 to 32767
Value set by Factory
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal