Alarm Summary

The
Alarm Summary
lists the alarms in a project or configured HMI device. Each project contains an
AlarmSummary
screen by default. Create an additional screen with an Alarm Summary graphic element to create a custom
Alarm Summary
screen.
The
Alarm Summary
lists alarms in the project that have the status of either
In Alarm
or
Unacknowledged
. View the
Details
pane of the
Alarm Summary
screen to see data such as Current Value, In Alarm Time, Out of Alarm Time, and tag values for the last selected alarm.
TIP:
For tag-based alarms, the Alarm Summary only displays alarms with
Use and evaluate alarm
selected in
Logix Designer
.
Use the
Alarm Summary
on an HMI device to:
  • Acknowledge alarms.
  • Disable alarms.
  • Shelve alarms.
  • Sort alarms.
  • Filter alarms.
  • Pause alarms.
  • Reset latched alarms.
  • View alarm details.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal