Change the order of columns in an Alarm Summary table
The columns of the alarm table on the predefined
AlarmSummary
screen appear in a default order. This screen is located in the Predefined Screens
folder of the Project Explorer
. To change the order of columns in an Alarm Summary table
- Point to the column card heading and select
- On the screen, select the Alarm Summarytable.
- In thePropertieswindow, select theColumnstab.
Move column up
or Move column down
to move the column higher (to the left) or lower (to the right) in the table. Changes made to the order of columns are depicted in the Alarm Summary table on the screen.
Provide Feedback