Delete a column from an Alarm Summary table
Delete a column to remove it from the Alarm Summary table. This removes unwanted data from the table and provides room for other data that may be more pertinent. You cannot change the data a column shows. By default, Column 2 in predefined Alarm Summary table of a project shows the alarm state. You cannot change column data from Alarm State to Comments or any other data.
To delete a column from an Alarm Summary table
- In the heading of the column card, select
- On the screen, select the Alarm Summarytable.
- In thePropertieswindow, select theColumnstab.
Delete
. Deleted columns are removed from the Alarm Summary table on the screen.
Provide Feedback