Add a column to an Alarm Summary table
New columns in an Alarm Summary table appear at the right side of the table with sample data inserted into each column. Sample data is representative of the length of data anticipated for a column. Use sample data to determine the column width to use for a column.
To add a column to an Alarm Summary table
- Select
- On the screen, select the Alarm Summarytable.
- In thePropertieswindow, select theColumnstab.
Add Column. - Select the data to display in the column. The selected column appears in the new card heading. Change the width of a column to display the data.
Provide Feedback