Change the width of a column in an Alarm Summary table
Change the width of a column in an Alarm Summary table if the data in the column is wider than the current width of the column. Use the sample data inserted in a column to determine the column width. The sample data is representative of the length of data anticipated for a column.
To change the width of a column in an Alarm Summary table
- On the screen, select the Alarm Summarytable.
- In thePropertieswindow, select theColumnstab.
In the- In the column card, clickShow/Hide
to expand the column card. The selected column card is outlined in blue.
Widthfield at the bottom of the column card, enter the value:- A positive number, representing the width of the column, in pixelsChanges to column width are saved automatically. The last column added fills the remaining space in the row. If the total width of all columns exceeds the width of the table, a horizontal scroll bar appears at the bottom of the table.TIP:When resizing a column in an Alarm Summary table, leave some space between the text of the column heading and the border of the column. If the text of a column heading appears at the column border, the text of the column heading may appear clipped in the Alarm Summary table on the HMI device
Provide Feedback