Alarm Summary table columns
On the
Alarm Summary Large
and Alarm Summary Medium
tables, alarm data appears in columns. To change an Alarm Summary table or when creating an Alarm Summary table, add columns (for example, add Severity or a row shown in the Details
pane of the alarm table as a column in an Alarm Summary table), remove columns, or rearrange columns. This table shows the default columns used in the Alarm Summary table on the predefined AlarmSummary
screen. Column | Description | Medium Alarm Summary | Large Alarm Summary |
! (Priority) | The urgency of the event:
| ||
Alarm State | The state of the alarm condition:
| ||
Inhibit State | The value applied to an alarm that inhibits the alarm at some level. These states include:
If no icon appears for Inhibit State, the alarm is of good quality and is not disabled, suppressed, or shelved. | ||
Event Time | The time the alarm condition or sub-condition changed to the currently displayed state. | ||
Condition Name | A name that describes the alarm condition. Condition names vary by event category. For example:
| ||
Alarm Name | The list of alarms, in all states, for the controllers referenced in the View Designer project. Each row contains an alarm and the conditions. Depending on configuration, the Alarm Name can appear as ::ControllerName.TagName or ::ControllerName\ProgramName.TagName. For tag-based alarms, the Alarm Name appears as ::ControllerName\ProgramName.TagName.@Alarms.AlarmName. If the tag is not located inside a program, this part is omitted and the Alarm Name appears as ::ControllerName.TagName.@Alarms.AlarmName. | ||
Message | The message assigned to the alarm in the alarm instruction. |
Provide Feedback
and Urgent