Details pane rows
Selecting
on an alarm table opens the
Details
on an alarm table opens the Details
pane in the lower half of:- Large Alarm Summary table
- Large Alarm Manager table
- Large Alarm History table
The
Details
pane replaces the list of alarms in medium alarm tables. The Details
pane shows details for the selected alarm condition of a selected alarm. Condition details display the selected alarm condition in the Alarm Manager table. The contents of the Details
pane appears in rows.Row | Description |
Priority | The urgency of the alarm condition:
|
Severity | The numeric value mapped to the assigned priority of the alarm condition:
|
Alarm State | The state of the alarm condition:
|
Inhibit State | The value applied to the alarm condition that inhibits the alarm at some level. These states, indicated by an icon in the alarm table, include:
These states can be combined. When an alarm has more than one inhibit state applied, the icon of the highest inhibit state shown above appears in the table. |
Event Time | The date and time the alarm event occurred. |
Condition |
|
Expression | The expression configured in Logix Designer for the selected condition. The expression appears only for tag-based alarms. |
Alarm Name | The name of the alarm. This name includes the controller name of the alarm and the tag name. It can also include the name of the program if the tag is defined at the program level. Depending on how it was configured, the Alarm Name can appear as ::ControllerName.TagName or ::ControllerName\ProgramName. For tag-based alarms, the alarm name can appear as ::ControllerName\ProgramName.TagName.@Alarms.AlarmName. If the tag is not located inside a program, this part is omitted and the Alarm Name appears as ::ControllerName.TagName.@Alarms.AlarmName. |
Message | The message assigned to the alarm in the Logix Designer project. |
In Alarm Time | The time the selected alarm entered the In Alarm state. |
Acknowledge Time | The time the selected alarm was acknowledged. |
Out of Alarm Time | The time the selected alarm entered the Normal or Out of Alarm state. |
Enabled Time | The time the selected alarm was enabled. |
Disable Time | The time the selected alarm was disabled. |
Suppress Time | The time the selected alarm was suppressed. |
Unsuppress Time | The time the selected alarm was unsuppressed. |
Shelve Time | The time the selected alarm was shelved. |
Unshelve Time | The time the selected alarm was unshelved. If the alarm is currently shelved, this is the time the alarm is unshelved automatically when the shelve duration expires. |
Alarm Class | The user-defined class assigned to the alarm in the Logix Designer project. |
Alarm Group | Displays the alarm group from Logix Designer to help classify and sort alarms. Displayed only for tag-based alarms. |
Limit Value Exceeded | The condition limit assigned to the alarm in the Logix Designer project. |
Tag 1 Value | The value of the associated tag parameter 1. |
Tag 2 Value | The value of the associated tag parameter 2. |
Tag 3 Value | The value of the associated tag parameter 3. |
Tag 4 Value | The value of the associated tag parameter 4. |
Alarm Count | The number of times the alarm condition has entered the In Alarm state. |
Current Value | The current tag input value resulting in the alarm state. |
Event Category | Digital events are categorized as Discrete. Analog events are categorized as Level. |
Shelve duration | The default time for which the selected alarm condition is shelved to prevent the notification of new state changes. Shelve duration is assigned to the alarm in the Logix Designer project. |
Max Shelve Duration | The maximum time the alarm can be shelved. |
Quality Details | Displays information of a fault in case of faulted alarms. |
State Change Type | This row applies to Alarm History only and displays the type of alarm state change for the currently selected alarm record:
|
TIP:
The Alarm History table does not contain the following details pane rows:
- In Alarm Time
- Acknowledge Time
- Out of Alarm Time
- Enabled Time
- Disables Time
- Suppress Time
- Unsuppress Time
- Shelve Time
- Unshelve Time
- Shelve Duration
Max Shelve Duration
Provide Feedback