Alarm Manager
The
Alarm Manager
lists all alarms configured in a system and their current states. By default, each project includes an AlarmManager
screen. Create an additional screen with a graphic element to create a custom Alarm Manager table.
TIP:
For tag-based alarms, Alarm Manager displays alarms marked as active and ready for evaluation.
Use the
Alarm Manager
to monitor and interact with the alarms on the HMI device. View the Details
pane of the Alarm Manager
screen to show all of the details of the selected condition.
TIP:
Refer to
Logix Designer
Help for the information about tag-based alarms.Provide Feedback