Alarm Manager table columns
The Alarm Manger table provides alarm information in columns:
Column | Description |
Alarm State | The conditions of the alarm:
The Alarm Manager table displays a combination of all the conditions of an alarm. If any condition in the alarm is In Alarm or Unacknowledged, the alarm appears as In Alarm or Unacknowledged in the Alarm Manager. |
Inhibit State | The value applied to an alarm that inhibits the alarm. These states include:
When an alarm has more than one inhibit state, the icon of the highest inhibit state appears in the table. If no icon appears, the alarm has good quality, and is not disabled, suppressed, or shelved. |
Alarm Name | The name of the alarm created in Logix Designer . For instruction-based alarms, it includes the alarm controller and tag. It can also include the name of the program if the tag is going to be defined at the program level. The Alarm Name can be configured as ::ControllerName.TagName or ::ControllerName\ProgramName.TagName. For tag-based alarms, the Alarm Name appears as ::ControllerName\ProgramName.TagName.@Alarms.AlarmName. If the tag is not located inside a program, this part is omitted and the Alarm Name appears as ::ControllerName.TagName.AlarmName. |
Provide Feedback
and Urgent