Specify access to operations performed on an Alarm Manager table
Specify which users have access to perform certain operations on an Alarm Manager table. For example, determine that all users, regardless of their assigned security role, have access to enable an alarm. To do this, set the
EnableAccess
property to Full Access
. Alternatively, determine that security access to enabling alarms depends on the role assigned to the logged in user. In this case, set the EnableAccess
property to Inherit
.To specify access to operations performed on an Alarm Manager table
- On the screen, select the Alarm Manager table.
- In thePropertieswindow, select thePropertiestab.
- Expand theSecuritynode.
- Locate the property for the button to set access:
- DisableAccess.Set access toDisable
on the selected Alarm Manager table. This button stops an alarm condition from being evaluated, effectively turning off the alarm. - EnableAccess. Set access toEnable
on the selected Alarm Managertable. This button allows an alarm condition to be evaluated, effectively turning on the alarm. - ResetCountAccess. Set access toReset Alarm Counts
on the selected Alarm Manager table. This button resets the Alarm Count value to zero on the alarm table. The alarm count indicates the number of times an alarm has gone into the In Alarm State. - ShelveAccess. Set access toShelve
on the selected Alarm Manager table. This button prevents the notification of new state changes for an alarm or alarm condition. - UnshelveAccess. Set access toUnshelve
on the selected Alarm Manager table. This button resumes the notification of new state changes for an alarm.
- In the box, select an option:
- Inherit.Specify that access to the button is inherited from the screen.
- Full Access. Specify that all users have access to the button.Inherited access for a user role can be Full Access, Read-Only access, or No Access. If a button inherits Read-Only access, hash marks appear across the button on the HMI device. Pressing the button displays an error. If a button inherits No Access from the screen, there is no access to the screen containing the alarm table. In this case, the screen does not appear in theNavigation menuon the HMI device.
Provide Feedback