Details pane for an Alarm Manager
In a medium Alarm Manager table intended for HMI devices with six-inch to nine-inch screens, the
Details
pane replaces the list of alarms in the table. In a large Alarm Manager table intended for HMI devices with ten-inch or larger screens, the Details
pane opens at bottom of the table. 
Item | Description | |
![]() | Buttons to shelve and unshelve the selected alarm condition in the Details pane when it is displayed at the bottom of the Alarm Manager table. | |
![]() | Shelve shelves the selected alarm condition in the Details pane. Shelving a condition prevents notification of new state changes to the alarm.Change the Shelve Duration and Max Shelve Duration through Logix Designer . If changes to the Shelve Duration and Max Shelve Duration values are not made through Logix Designer , the updated values are not propagated to the Alarm Summary and Alarm Manager clients. In this case, the previous Shelve Duration and Max Shelve Duration values are used when shelving alarms in Studio 5000 alarm tables. | |
![]() | Unshelve unshelves the selected alarm condition in the Details pane. Unshelving a condition allows notification of new state changes to the alarm. | |
![]() | Select a condition to show all of the details of the condition in the Details pane. For example, to show details for the TRIP condition for the selected alarm, scroll to and select TRIP. | |
![]() | The condition details for the selected alarm. The details include when the alarm condition was enabled or disabled, suppressed or unsuppressed, or shelved. When multiple alarms are selected in the Alarm Manager | |
Provide Feedback