Disable a button on an Alarm Summary table
Prevent users from performing certain operations on an Alarm Summary table on the HMI device. To do this, disable the appropriate button on the alarm table. For example, to prevent disabling alarms, disable
for the Alarm Summary table.
Disable
for the Alarm Summary table. On the HMI device, a disabled button has diagonal hash marks across it. Tapping the button displays an
. Tap the
Error
icon
. Tap the Error
icon to open an Error list that describes the button as disabled. To disable a button on an Alarm Summary table
- On the screen, select the Alarm Summary table.
- In thePropertieswindow, select thePropertiestab.
- Expand theGeneralnode.
- Clear the check box to disable the button and the associated operation on the HMI device:
- AcknowledgeEnabled. Clear this check box to disableAcknowledge
on the selected alarm table. This prevents indicating awareness of the alarm and changing the alarm state from unacknowledged to acknowledged. - DisableEnabled. Clear this check box to disableDisable
on the selected alarm table. This prevents stopping an alarm condition from being evaluated, effectively turning off the alarm. - ResetLatchedEnabled. Clear this check box to disableReset Latched Selected
on the selected alarm table. This prevents resetting a latched alarm that is latched in the In Alarm state. - ShelveEnabled. Clear this check box to disableShelve
on the selected alarm table. This prevents stopping the notification of new state changes for an alarm or alarm condition.
Provide Feedback