The Graphics editor
When you start the
Graphics
editor you see a window with various menus, toolbars, and palettes, and a display window (drawing area) where you create and edit a graphic display.If you select an existing display when you start the editor, the display determines the size of the editor's window.
Replace displays use the size specified in the Project Settings editor.
You can specify the size of On Top displays individually in the Display Settings dialog box or using the handles on the dotted line surrounding the display.
TIP:
You can have multiple graphic displays open at one time.
Project settings affect how your graphic displays look. Specify project settings before you create graphic displays.
Provide Feedback