Save and exit from the Graphics editor

To save the graphic display you are working on and close the Graphics editor
  1. Choose
    Save
    from the file menu or click the Save tool in the toolbar. This saves the graphic display with its existing name.
    To save a previously saved graphic display under another name, choose the
    Save As
    command. This creates another copy of the display with the new name.
  2. Choose Close from the
    File
    menu.
    If you haven't saved your changes, you'll be asked if you want to.
    • Answer Yes to save the graphic display.
    • Answer No and all changes will be discarded.
      TIP:
      When renaming graphic displays, make sure you update any graphic objects that use the display name (for example, go to display button or display list selector) to the new name.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal