Set up display properties and behavior
Use the
Display Settings
option on the Edit
menu to set up how the current graphic display will look and behave at runtime.To set up the display properties and behavior
- ChooseDisplay Settingsfrom theEditmenu.
- In theGeneraltab, specify the details of how the display will look at runtime.
- In theBehaviortab, specify how the display will behave at runtime.
- ClickOKwhen the settings are complete.TIP:If the tags assigned to a graphic object have not yet been scanned or are in error, the object will appear in the display with an outline, or will display some special form, such as asterisks, to indicate an error.
Provide Feedback