Edit display behavior settings (Behavior tab)

To edit the runtime behavior settings for a display
  1. Click the
    Behavior
    tab in the
    Display Settings
    dialog box.
  2. Edit the settings presented in this tab.
Macros
In these boxes, enter macros that will run when a display is started up or shut down.
  • Startup
    Click the
    Browse
    button and select the macro that is to run when the display is opened, or type the macro in if you are sure of its spelling.
  • Shutdown
    Click the
    Browse
    button and select the macro that is to run when the display is closed, or type the macro in if you are sure of its spelling.
Behavior of Object with Input Focus
Some interactive objects need to be selected by tabbing to them or clicking with the mouse to activate them so they have input focus. Among the objects that require this sort of activation are alarm lists, trends, and display list selectors.
  • Disable Highlight When Object has Focus
    Check this box to turn off the highlighting of the object with input focus.
  • Highlight Color
    Choose the color of the highlight displayed at runtime around the object that currently is active and has focus.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal