Edit graphic displays

A graphic display consists of drawing objects such as ellipses and rectangles; interactive objects such as push buttons, numeric displays, and control list selectors; ActiveX objects provided by other applications; and display settings.
To edit an existing graphic display
  1. Open the
    Graphics
    folder in the
    Explorer
    window.
  2. Open the
    Displays
    list.
  3. Double-click the name of the graphic file to edit.
  4. Use the tools and menu options available in the
    Graphics Display
    editor to modify the graphic display.
  5. Save the graphic display. If you are editing a graphic template as the basis for a new graphic display, select
    Save As
    to give the graphic display a new name.
    TIP:
    • To see the menu options available for any object on the graphic display, right-click the object.
    • To see display settings, right-click a blank area of the display and select
      Display Settings
      .
    • To open the editor’s toolbars, select them from the
      View > Toolbars
      menu.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal