Specify grid settings for a display
A grid helps you size and position objects precisely. You can change the grid settings any time while you are drawing. You can also use the
View
menu items Show Grid
to turn grid visibility on and off, and Snap On
to activate or de-activate the grid.To set up the grid for a display
- SelectGrid Settingsfrom theViewmenu.
- Select the attributes and spacing for the grid.
- ClickOK.TIP:Font sizes are not given in pixels. If you want to place text on the grid lines you will have to make the vertical grid slightly larger to accommodate the font. For example, if the font size is 10, and the grid is 10 x 10, the font will not fit correctly. If you make the grid 10 x 16, increasing the vertical grid by 6 pixels, a size 10 Arial font will fit. The amount you have to increase may vary from font to font.The grid settings apply to all subsequently opened displays.
Options
- Attributes
- Show GridClick to make the grid visible.
- Snap To GridClick to make the grid active. When the grid is active, all the objects you draw, except freehand objects, are pulled to the closest grid point.
- Grid ColorSelect a color for the grid points.
- Spacing
- Horizontal (x)Set the horizontal (or x axis) spacing for the grid points in pixels.
- Vertical (y)Set the vertical (or y axis) spacing for the grid points in pixels.
Provide Feedback